AXIS#.IL.COGCOMP.MOVETOSTART.V
Description
Sets the velocity used when moving the axis to the Teach Start Position (AXIS#.IL.COGCOMP.TEACH.POSSTART).
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-08-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value | 1 rpm |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.IL.COGCOMP.MOVETOSTART.V | 0x500A | 0x26 | UINT | 1:1 | Velocity | RW | False |
AXIS2.IL.COGCOMP.MOVETOSTART.V | 0x510A | 0x26 | UINT | 1:1 | Velocity | RW | False |